请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ27Z561-R1 主题中讨论的其他器件:BQSTUDIO、 BQ27Z561、 EV2400
现在、当读取0x3E 的块内容、例如0x0006时、读出的值为43 12、这与官方网站提供的10 12不一致。 此外、当读取块数据时、IIC 的时钟频率不能超过10kHz、并且如果数据超过10kHz、则将会无序
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.