请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61178 大家好、
客户希望了解 TPS61178在为2节3400mAh 锂离子电池充电时的温度。 输入电压为6V 至8.4V、输出电压为12V 和20V、充电电流介于1.5A 至2A 之间、功率输出为20W-30W。
此致、
Danilo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.