Other Parts Discussed in Thread: TPS2595
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2595 尊敬的先生:
我们知道通过2个电阻分压器设置 TPS259573 OCP、但如何计算它?
例如:如果需要3.8V 电压、如何使用 R1和 R2?
谢谢、Ian。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.