请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5060 锁定"LM5060:想法检查"的后续问题
由于 每个电池的电压可能会变化、因此可能是电压最高的电池为整个系统供电。 如果断开此电池、此 LM5060 + LM74700解决方案是否能够无缝切换至其他电池而不会中断输出功率(例如显著的压降)、是否需要在输出端使用超级电容器、因为最大电流为150A?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.