您好!
我的客户使用 ULN2003A 来驱动7个电子阀。 它们需要同时3个通道输出 、以在50%占空比下支持750mA、其他通道
但根据下面的曲线、 在这种情况下、每个通道的峰值电流只能输出超过200mA 的电流、非常接近750mA 的裕度。
他们更喜欢小型封装、您是否会建议这 种封装是否可行? 或推荐其他器件。 谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.