请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:UCC28951您好!
建议使用适用于3.3KW 车载充电器的控制器 IC。
合适的拓扑。
输入为(PFC 之后):390V -410V DC
输出电压:45V 至65V DC
输出电流:50A DC
此致、
Sathish。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.