请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS55288 大家好、
是否有可满足以下要求的降压/升压转换器:
- 输入电压为4V 至12V
- 良好的动态输出特性,因为输入电压将从9V 下降到4V,
- 恒定输出电流约为4A。
- 所需的外设电感器高度小于1.2mm
TPS55288是否最符合这些要求? 或者还有其他产品适合这些产品吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.