请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS7A8101 大家好、
对于 TPS7A8101、在数据表表表2中、我们没有看到输出电压为4.5V 的 R1和 R2值。
VIN 为5V、您能否为 Vout= 4.5V 提供 R1和 R2值?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.