Other Parts Discussed in Thread: LM2596, LM2597, LM2595
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM2596 主题中讨论的其他器件: LM2597、 LM2595
您好、E2E、
绝对最大额定值表中写入了 SD/SS。 开/关引脚是否意味着相同?
此致、
ACGUY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM2596只有一个用于控制器件的"开/关"或"关断"控制。
该系列中的其他器件、例如 LM2597、具有更多功能;例如组合关断和软启动引脚、称为 SD/SS。
LM2596和 LM2595具有简单的开/关功能、无需外部软启动。 LM2596和 LM2595开/关引脚的额定值为-0.3V 至
25伏。 对于 LM2597 SD/SS 引脚、电压为6V。 LM2596数据表的不同版本似乎会引起混淆。