请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS23881 你(们)好
TPS23881是否具有电源序列规格?
由于电流输入电源54V 输入的上升时间相对较长、因此先提供3.3V 电压、有时 PoE 不工作。
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.