Other Parts Discussed in Thread: TL431
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TL431 你(们)好
TI 431系列的最高耐受电压似乎仅为36V。
由于输出电压需要超过60V、因此必须将其添加到 TL431反馈电路的稳压器中。
我想问、是否有更高的耐受电压431 (或也可以使用相关的应用材料)来避免使用额外的稳压器电路。 谢谢。
此致、
摇滚
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.