请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2491 主题中讨论的其他器件:TPS2490
您好!
数据表6.1注释(2)指出:"OUT 将在1ms 或更短的时间内承受-2V 的瞬变。
在我的客户板上、输出瞬变在~10us 内变为-4V。
这种损坏可以是 TPS2490还是应该正常?
此致、
希拉诺
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.