Other Parts Discussed in Thread: LM5170
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5170 你(们)好,先生
我需要一个功率级
规格为输入电压48V
输出电压为0.5V~6V/60A
LM5170是否是合适的解决方案?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.