请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:REF3425 大家好、团队、
输出电流为2mA 时、REF3425的最大压降是多少? 遗憾的是、数据表在0mA 时仅规范100mV、在10mA 时仅规范500mV/10mA。 我们的预算在2mA 时为250mVmax。
非常感谢
Lutz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.