请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS63070 您好!
TPS63070数据表 P6、7.5电气特性、VIN 测试条件中描述的"启动后;Vout >= 3.0V"和"启动时;Vout < 3.0V"是什么意思?
这是否意味着启动时至少需要3.0V 电压?
此致、
Nishie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.