Other Parts Discussed in Thread: TLV757P
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TLV757P 我尝试在 VIN=1.8V 的情况下从 TLV757P 生成1.2V@800mA。 根据数据表、图14和15显示了3.3V 和5V 输入电压。 当 VIN=1.8V 时、压降是多少、或者如何估算?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.