请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ77915 对于过流保护设置、如果我使用的电阻值接近列出的值、但容差为10%而不是1%。 会发生什么情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对于过流保护设置、如果我使用的电阻值接近列出的值、但容差为10%而不是1%。 会发生什么情况?