请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:UCC28C41是否有人可以建议我可以为单开关隔离式正向直流/直流转换器选择哪种 IC?
以下是我的参数要求:
输入电压 :0至24V (直流)
输出电压 :15V (直流)
最大输出电流 :1A
开关频率:100kHz
隔离 :4千瓦
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.