请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ76930 主题中讨论的其他器件:TIDA-00792、 BQ78350
尊敬的 TI 支持团队:
根据,我有疑问,请使用3.3V LDO (TS1)源作为 LED 的直接电源(总电流~12mA)。 根据数据表的最小限制为30mA,但根据 EVM 和 TIDA-00792,您的实施是通过源跟随器实现的。
B.R
Alexander Burtakov
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的 TI 支持团队:
根据,我有疑问,请使用3.3V LDO (TS1)源作为 LED 的直接电源(总电流~12mA)。 根据数据表的最小限制为30mA,但根据 EVM 和 TIDA-00792,您的实施是通过源跟随器实现的。
B.R
Alexander Burtakov