请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS53355 各位专家:
我的应用是将12V 电压转换为3.3V 电压、负载为20A。
除了从12V 除以电压之外、我还可以使用"VREG"来启用 TPS53355本身吗? 是否存在任何风险或限制?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.