请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TL431、 TLV431尊敬的 TI:
我的客户需要一个解决方案、以实现-100mV Vin,输出电压需要实时调整。 Vout=-70mV、-60mV,-50mV 等, 每个输出的差值为10mV。
是否 有任何解决方案建议? 谢谢!
此致!
沈家祥
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.