请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM137 您好!
我想检查一下以下内容:
如果 LM137的输入为-7V、输出为-5V、负载电流为1A、则器件的功耗是否为~¦(-7 --5)*1¦= 2W?
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.