请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS563201 您好!
TPS563201的最高工作温度 Tj 150°C、但热关断温度。 172°C、TI 能解释一下吗? 谢谢你。
C.T.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.