请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM3410 大家好、
请帮助检查原理图、尤其是输出电容器。
我们认为、在常见的直流/直流应用中、输出电容器 nF 电平非常小、但根据数据表中的公式28、30、结果为 nF。
我们的 Vin=3.3V。 LED VF 如下所示、Vout=4.04V。 效率= 0.9。 fsw=1.6米。 LED 动态电阻= 2。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.