请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS54360 尊敬的 TI 团队:
TPS54360的输入为6V-36V、输出为12V。
当输入为6V、输出为12V 时、TPS54360是否会损坏? EN 引脚为高电压。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.