请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ27426 你(们)好
BQ27426的设计容量为14000 mAh、但规格为8000 mAh。 哪一个是正确的?
我们并联使用三节18650电池、总容量为10、000mAh。
BQ27426是否可以支持它?
谢谢你。
Jerry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.