请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS63036 数据表中给出的引脚 FB 上的电压容差仅适用于室温(数据表第3页)。 为了 进行误差分析、我需要知道整个工作温度(-40至85C)范围内的容差(或温度系数)。 你可以帮帮我吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
数据表中给出的引脚 FB 上的电压容差仅适用于室温(数据表第3页)。 为了 进行误差分析、我需要知道整个工作温度(-40至85C)范围内的容差(或温度系数)。 你可以帮帮我吗?