请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMR62014 输入电压是一个典型的2节锂聚合物电池、电压范围为6.3V~8.4V。 目标电压输出为12V。 因此、我将设计从带上拉电阻器的 webench 复制到了50k、并用 ss34替换了二极管。 但是、输出电压不是12、而是7 (有时输出正确)、有时测量的反馈引脚电压为5.3~7。 lmr62014无法输出电压的原因是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.