请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP5018 根据 LP5018数据表、由于每个通道电流都由连接到 IREF 引脚的 Rref (R8=3.9K)设置、因此请验证此原理图并确认需要150 Ω 和100 Ω 的串联端接电阻器、或者我们可以将其设置为0 Ω。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.