Other Parts Discussed in Thread: TPL7407LA
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPL7407LA 由于设计限制、我想将 COM 连接到5V。
每通道的输出电流设计为20mA。 如果 COM 引脚连接到5V、那么 RDSon 和 VOL 是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.