Other Parts Discussed in Thread: LM66100
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61220 主题中讨论的其他器件:LM66100
大家好、
我的客户想知道数据表第一页上的"最小开关电流200mA"是什么意思。
在下面的应用部分中、我们可以将 IO 从100uA 应用到50mA。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.