请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2121 当 IN2处于活动状态时、电压为0.0 V。 (这符合预期)
当 IN1激活时、引脚 PWR_MUX_ST 上的电压为0.78V。 (我希望电压为5V)
有人能帮你解决原因吗?
谢谢、
Ashish
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
器件型号:TPS2121