请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TLC5955 团队、
此器件的最快更新速率是多少?
对于串行输入、最快时钟速度为25MHz。 因此、假设我将1MHz 数据传输速度和16位数据传输速度用于所有48个输出、即:
(1/(1 MHz)*16位*48输出=768微秒?
谢谢
Viktorija
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
团队、
此器件的最快更新速率是多少?
对于串行输入、最快时钟速度为25MHz。 因此、假设我将1MHz 数据传输速度和16位数据传输速度用于所有48个输出、即:
(1/(1 MHz)*16位*48输出=768微秒?
谢谢
Viktorija