请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61281 主题中讨论的其他器件: TPS61022
你(们)好
您能否帮助查看 TPS61281是否支持 输入电压3.0V~4.1V、 输出电压:4.2V 和输出电流(最大值) 2.5A?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.