您好、专家、
TPS54428是否存在最大软启动时间规格限制?
谢谢。
Allan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、Allen、
我看不到您在3.3V 时无法获得正确输出电压的任何原因。
除了将 CPC24更改为8200pF 之外、您还可以尝试删除 CPC25、然后查看是否可以获得正确的输出?
在 WEBENCH 上、建议最短软时间为1.15ms。
此致、
简森