Other Parts Discussed in Thread: BQ24130, BQ25798
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24130 主题中讨论的其他器件: BQ25798
您好!
数据表规定、该器件可在4.5V 至17V 的电压范围内运行。
为了给3节电池(12.6V)充电、我是否需要提供至少13.5V 的电压、或者它是否能够在5V 电压下工作?
谢谢、
体层器
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.