请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS92391、 TPIC6B595大家好、
您能否帮助为以下输入选择合适的 LED 驱动器?

VBAT=24V、(如果=100mA、VF=2、9V、每个 LED) 6x8或8x6 LED 灯串
我希望你能提供帮助。
此致、
Marvin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.