请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24232 您好!
我有一个4.35V 电池、我想知道是否有一个与 BQ24232类似的器件可以为电池充满电。
我查看了 BQ24232器件、它看起来只能为电池充电4.2V。
此致、
Gautham
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.