请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM2682 主题中讨论的其他器件: LM2775、 LM2681
大家好、
我们是否有任何器件可实现以下功能?
VIN=3.3V/5V
Vout1=8.5V 20mA,Vout2=10V 2mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.