请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS23881 您好,
客户想要检查 TPS23881 60W 和90W、请帮助检查 端口注入器、如下所示:
1、不需要 U2/U3/U4 IC、对吧?
2.如何按如下方式设置 TPS23881引脚44、45、53、54、55、56:
此致、
LIN
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.