请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS65911 您好!
上电时、我们尝试通过 I2C 通信将 VDD1-SMPS 输出电压设置为1.35VDC、但有时会将其输出设置为2.7VDC。
是否发布了与此电压增加问题相关的勘误表/公告?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.