TPS53667提供了一些电阻器值表、用于通过引脚搭接进行器件设置。 FSW、转换率、每相电流限制和引导电压等...
这些设置需要多大的电平电阻器容差? 5%是否正常? 需要1%或1%?
在 EVM 上、射频电阻值为30.1k 欧姆1%电阻。 对于500kHz 设置、电阻器表值为30k Ω。 因此、我认为允许使用5%的电阻器。
此致、
Kohei Sasaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.