Other Parts Discussed in Thread: TPS40425
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS40425 你(们)好,先生
TPS40425是否需要检查环路增益?
从 EVB 表中、我们需要向 R8 (EVB)注入信号、我们需要多少信号电压? 也是10mV?
我们需要设置什么频率范围?
令人很烦
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.