Other Parts Discussed in Thread: TPS61022
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61022 大家好、
如果我们选择 TPS61022、则支持的最大持续输出电流是多少?
在我们的应用中、我们需要连续使用4V、5.5A。
请尽快提出建议。
谢谢
Saumil
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.