请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5001 输入电压为12V-24V、输出电压=40V、输出电流=20mA。工作时间长、输出电压偶尔下降到10V 以下、电感(L1) 发出啸叫声。我将 L1从6.8uH 更改为150uH、问题仍然存在。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.