请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM3478 你(们)好
LM3478上是否有最小负载。?
空载时、电压摇晃。周期为168Hz。
条件如下。
输入13V~18V
输出12V
SEPIC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.