Other Parts Discussed in Thread: TPS61230
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61230 现在、我们开发了一个计算机表、希望使用 tps61230为3.3V、3.8V、5V 输入提供电源、2.8V 至5.5V、该芯片组可以正常工作?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.