请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25882 主题中讨论的其他器件: BQ25713
您好!
我想设计电池管理、它可以为2节锂电池充电。
我的系统需要至少7 - 8伏和3A。
BQ25882是否可以在系统系列上支持它?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.