Other Parts Discussed in Thread: LM5163, LM5166, LM76002, TPS65131, TPS65130
您好!
您能否推荐一种支持24V 输入[48V 峰值]和三路输出5V (2.5A)、15V (1.5A) 、-15 (200mA)的解决方案。
。器件越少、T Ü V S Ü D 就越好。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的 Yue:
对于5V 和15V 输出、您可以考虑使用 LM76002/3。 15V 是通过配置为反相降压/升压的降压转换器实现的-在给定此处所需的电流电平时、请考虑 LM5166 65V/0.5A 或 LM5163 100V/0.5A 转换器。 请注意、反相降压/升压所需的输入电压额定值为 Vin + Vout = 48V + 15V = 63V。 WEBENCH 可帮助您完成这些设计。
此致、
Tim