Other Parts Discussed in Thread: TPS51206
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS51206 你好。
S3和 S5的高输入信号是否可以通过电阻实现3.3V 电压?
VDD 为3.3V。
VDDQ 为1.5V。
此致、
DIE-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.